• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Data Converters » Video Converters » Video Converters - Forum » All Tags » video decoder
Share
Video Converters
  • Forum
  • Announcements

Browse by Tags

Video Converters

Welcome to the Video Converters Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
video decoder
  • A/D converters
  • Camera
  • capture
  • color
  • DM365
  • encode
  • NTSC
  • PAL
  • RGB
  • TVP5146
  • TVP5146M2
  • TVP5147
  • TVP5150
  • TVP5150A
  • TVP5150AM1
  • TVP5150BPS
  • TVP5151
  • TVP5154A
  • TVP5158
  • TVP7002
  • VGA
  • Video
  • Video ADC
  • Video Quality
  • YCbCr
Related Posts
  • Forum Post: TVP5150 video decoder in non-standard application

    Dave Jones Dave Jones
    I need to lock to a standard definition video signal (NTSC or PAL) and generate a line locked pixel clock, H sync, V sync, composite blanking and color subcarrier. The TVP5150 looks like it can do all of that except recreating the color subcarrier. I can not find any chips in current production that...
    on Aug 4, 2009
  • Forum Post: TVP5150AM1 no NTSC colour lock

    David Ambry David Ambry
    Hi there, My TVP5150AM1 application does not colour lock on NTSC, but does on PAL. Luminance is always correctly decoded. Sometimes Pr is correctly decoded, but in that case there is no Pb. Some background information: The device is clocked from the crystal output of a 3.3V 8051-family...
    on Aug 17, 2009
  • Forum Post: Re: Line ID - An issue about TVP5158!

    Viet Dinh Viet Dinh
    Leon, The line ID can be larger or smaller than standard number of line if: The input signal is non-standard The input is pulled in/out when it is in the middle of the field. The line count does not reset until it detects a vsync. So, the backend can ignore the line ID that is greater than...
    on Apr 9, 2010
  • Forum Post: Re: TVP5158 loss the sync when IR camera is used and turn on IR lamp

    Viet Dinh Viet Dinh
    SI, To check for the patch download correctly, you can read the RAM Version (register 05h) and RAM Test Version (register 06h). For example, if the patch is 02.01.17, you should get 01 for register 05h and 17h for 06h. We will try the sync loss in lab. Regards, Viet
    on Apr 13, 2010
  • Forum Post: TVP5150 question

    ZHENGXU HUANG ZHENGXU HUANG
    HI, all I am using TVP5150A connecting with a PAL camera as input, and connect to DM642.The TVP5150 output is a standard ITU-R 8bit BT656 4:2:2 (720*576) with embedded synchronization(SAV and EAV).The DM642 is used to process the BT656 data.ALL function is OK .However the output video has a black...
    on Jan 11, 2010
  • Forum Post: Re: Problem Using a TVP5150AM1 in PAL Mode

    seunghun lim seunghun lim
    Dear Viet, Thank you for your reply. I applied V048CAA patch but still have same problem. After using patch, check ID results are; ROM major version 82h -> 04h ROM minor version 83h -> 8ch Do you have another recommendable try? Regrads, Sam
    on Dec 3, 2010
  • Forum Post: Re: Problem Using a TVP5150AM1 in PAL Mode

    seunghun lim seunghun lim
    Dear Viet, The register 8Ch is 83h(Autoswitch mode and (B,G,H,I,N)PAL ITU-R BT.601). By the way, the Status register #1(address 88h) value is read 6Eh or EEh(Peak white is detected or not). Especially the picture such as posted in my previous question, EEh is read more frequently than...
    on Dec 6, 2010
  • Forum Post: Problem Using a TVP5150AM1 in PAL Mode

    seunghun lim seunghun lim
    Hi, Everybody. I faced problems using a TVP5150AM1. I am developing a car AVN with PLDS Loader + TCC8900 CPU(Telechips). In NTSC mode, there is a little bit flicker noise also. But in PAL mode, there are lots of flicker and 'Rainbow' effect(Please, forgive me. i don't know the...
    on Dec 1, 2010
  • Forum Post: Re: Migration from TVP5150AM1 to TVP5151

    Tetsuro Fukuhara Tetsuro Fukuhara
    Viet, Thanks for the answer. Could we say below? TVP5151 ROM SW = TVP5150AM1 ROM + TVP5150A_v048CAA patch I will let my customer to evaluate other minor SW changes on TVP5151 in addition to ones above. Best regards, T. Fukuhara
    on Jan 17, 2011
  • Forum Post: Migration from TVP5150AM1 to TVP5151

    Tetsuro Fukuhara Tetsuro Fukuhara
    Hi, Is there an official TVP5151 migration note from TVP5150AM1 for customers? May I say the customer can simply replace them on their current TVP5150AM1 boards without any register setting changes? Best regards, T. Fukuhara
    on Jan 13, 2011
  • Forum Post: Re: TVP5158 Scaler Half-D1 output

    Tetsuro Fukuhara Tetsuro Fukuhara
    Larry, Thank you for the horizontal scaling answer. How about the vertical scaling in case of CIF? Does it use any line filter, or just feild 1 only? Best regarfds, T. Fukuhara
    on Jan 21, 2011
  • Forum Post: TVP5151: interrupt on WSS change

    Andrea Pastega66071 Andrea Pastega66071
    Hello. I'm using a TVP5151 as video decoder, and enabled the WSS function to detect video format from input composite signal. It works and I can successfully read from the 0xC6 register that WSS data is available and I can read the WSS data from 0x94 registers. I tried to enable "data...
    on Sep 9, 2011
  • Forum Post: TVP5150AM1 - "Curling" Video

    Drew Rainwater Drew Rainwater
    Hello, I'm using the TVP5150AM1 with an NTSC source, outputting to an LCD. Occasionally, I'm seeing the top several lines of the output "curl" to the right. It always seems to be at the top of the video, and may be dependent on the content of the image, but it's hard to tell...
    on Sep 22, 2011
  • Forum Post: Converter ITU-R BT601 (16bits) to ITU-R BT656 (8bits)

    Juliano Felix de Abreu Juliano Felix de Abreu
    Hello, I have been working with the OMAP DM3730 that support BT656, the problem is that my camera is LVDS (ITU-R BT601), in other words, the input is 8bits to Y and 8bits to CbCr with VD, HD, CLK and Field. This way I need a converter ITU-R BT601 to ITU-R BT656 8bits to YCbCr with EAV and SAV included...
    on Nov 16, 2011
  • Forum Post: TVP5146 settings to extract 640x480 image size

    Navin Reddy Navin Reddy
    Normal 0 false false false EN-US X-NONE X-NONE MicrosoftInternetExplorer4 ...
    on Aug 22, 2011
  • Forum Post: Failed to encode video buffer

    doron sandroy doron sandroy
    Hi Larry I work on DM365/8 card and TVP7002 the componnent input work fine. i add new res/STD 600/800 rgb from CH 3 i the TVP7002 and add config to the tvp7002.c : if (res==600)//600/800 rgb svga { //TVP7002 set to convert RGB to YCbCr err = tvp7002_write_reg(sd,0x01,0x42); // 67); //...
    on Dec 29, 2011
  • Forum Post: TVP5150 Horizontal Offsetting Problem

    Luiz Fernando Ribeiro de S�� Luiz Fernando Ribeiro de S��
    I'm currently working in a project with arm9 and the TVP5150AM1, and i having a very strange issue, when i connect and disconnect the video signal cable from TVP5150 CVBS input, occasionally the video offsets horizontally, i observed that some noise on input can cause the same issue. I'm...
    on Feb 16, 2012
  • Forum Post: TVP5154A Vertical sync & Horizontal sync locking issues (Reg 88h)

    Prabul Kanth P M Prabul Kanth P M
    Hi, I am using Bitec Quad Video Card with TVP5154A as my Video decoder. I am not able to get the Vertical sync & Horizontal sync lock bits in register 88h as 'locked'. what could be the issue here?
    on Mar 19, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use