Dear All,
My customer is having problems with the TVP5150 and do have the following questions because it looks like they will have to turn-off the TVP5150 temporarily:
- What are the possibilities to turn the device off?
- Because they do not have a signal line to turn it off via the PDN-pin, Audi is wondering whether there is a possibility to do this via I²C:
- What happens when setting the register 02h, bit0, power down mode? will the oscillator continue to run? Is the PLL still on? Can the emission of the 27MHz radiation be reduced?
- What happens when setting the register 05h, bit0, software reset? Will this cause a short system reset only or can it be kept in reset for a longer time?
Thanks and regards,
Armin