Hi,
We are developing a custom board using TVP 5150.
We are entering camera images on our board. I want to detect that the camera is down at this time.
Can you detect that the video has expired with TVP 5150?
Regards
Hideki
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
We are developing a custom board using TVP 5150.
We are entering camera images on our board. I want to detect that the camera is down at this time.
Can you detect that the video has expired with TVP 5150?
Regards
Hideki
You can use the H-lock status (register 0x03 bit 4). This can be read from the register and/or directed to an output pin. Note this indicates the current status. There are also a sticky 'changed' indicators for H, V, rate and color lock in register 0x1D and are cleared by writing to register 0x1C.
The color lock can also indicate if the color sub-carrier has changed (i.e. the camera switched from color mode to monochrome mode).
Regards,
Steve