• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Data Converters » Video Converters » All Tags » TVP7002
Share
Video Converters
  • Forum
  • Announcements

Browse by Tags

Video Converters

Welcome to the Video Converters Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
TVP7002
  • A/D converters
  • ADC
  • capture
  • Colour
  • DM365
  • DM368
  • DM6467
  • encode
  • PAL
  • Problem
  • RGB
  • SN65LVDS315
  • ths8135
  • ths8200
  • tvp5146m2
  • tvp5147m1
  • tvp5150am1
  • tvp5158
  • TVP70025
  • tvp70025i
  • VGA
  • Video
  • video decoder
  • Video Quality
  • YCbCr
Related Posts
  • Forum Post: TVP7002 RGB TO YPBPR

    NINGMENG CHEN NINGMENG CHEN
    We connected TVP7002 to DM6467. Now the VESA(1280x720x60@R,G,B) video was converted by TVP7002 to 4:2:2 YCbCr data. We now found a problem about RGB2YCbCr mode. The "green" seems "black" The "blue" is very "blue" The "white" is also ok The "red"...
    on Jun 2, 2009
  • Forum Post: TVP7002 handling of VGA resolutions coming from component input

    Nir Aloni Nir Aloni
    I currently use the DM6467 EVM which has TVP7002 in its component video input. I noticed that when I connect a source which outputs 800X600@60 resolution to the EVM component input, the TVP7002 identifies this resolution as 720P as indicated by its 'lines per frame' register (lines per frame...
    on Jun 23, 2009
  • Forum Post: Re: TVP7002 handling of VGA resolutions coming from component input

    Larry Taylor Larry Taylor
    The TVP7002 required a VSYNC event to update lines per frame status. It is possible that the MUX for selecting the VSYNC input pin is not set correctly, following the swich to a graphics format. If a VSYNC event is not detected, the lines per frame status will not update and could contain old data from...
    on Jun 23, 2009
  • Forum Post: Re: TVP7002 handling of VGA resolutions coming from component input

    Nir Aloni Nir Aloni
    There is one thing I didn't mention in my previous message, which does not settle with your explanation: When I change the refresh rate of the 800X600 resolution to 200HZ (in the source connected to the component input), the 'lines per frame' changes to indicate 1080 lines. How is this...
    on Jun 23, 2009
  • Forum Post: Re: TVP7002 handling of VGA resolutions coming from component input

    Larry Taylor Larry Taylor
    After switchinging to the 200Hz source, what is the line count after toggling SP RESET?
    on Jun 23, 2009
  • Forum Post: Re: TVP7002 handling of VGA resolutions coming from component input

    Nir Aloni Nir Aloni
    One correction - the inidication for 1080 lines happens when I set resolution to 1024X768@200Hz . Anyway, I added toggling of SP reset and even then the indication in 'lines per frame' is 1080, i.e. value of 0x465.
    on Jun 24, 2009
  • Forum Post: Re: TVP7002 handling of VGA resolutions coming from component input

    Nir Aloni Nir Aloni
    Any explanation to the above TVP7002 problem?
    on Jun 25, 2009
  • Forum Post: Re: TVP7002 handling of VGA resolutions coming from component input

    Larry Taylor Larry Taylor
    We do not have have a true XGA 200Hz source, but when an XGA 60Hz progarmmable source was used with VSYNC set to 200 Hz (HSYNC left at 48.363KHz), the line count read back was 242 as expected (60/200x806lines). The TVP7002 EVM was used for this test Are both graphics and HD sources connected to the...
    on Jun 25, 2009
  • Forum Post: Re: TVP5150AM1 no NTSC colour lock

    Kevin Chalmers Kevin Chalmers
    Dave, Are you using this device with a YPbPr input? If so, that may be your issue. The TVP5150 is a composite, Svideo analog video decoder. It does not support component or YPbPr video inputs. You will need a TVP7002 video triple ADC to digitize Y/Pb/Pr. Hope this helps. Regards, Kevin
    on Sep 11, 2009
  • Forum Post: Converting Analog S-Video to Digital RGB Data for FPGA Interface

    Aditya Satpute Aditya Satpute
    Hi , I am looking for a low power video ADC , which can convert the S-video information to corrosponding digital information. I need to interface the same to an FPGA . I have the s-video image source as a camera (PAL) and i am now looking for the video ADC. I have been suggested TVP7002 . Has some1...
    on Nov 5, 2009
  • Forum Post: Re: TVP7002 question

    Larry Taylor Larry Taylor
    David, DIV2=1 has been used for ADC testing, and in some cases it is used with 2x HPLL feedback divider to improve PLL jitter. When used with a 2x HPLL feedback divider (2x total pixels per line) the horizontal resolution will be unchanged. When used with 1x HPLL feedback divider (standard total...
    on Jun 7, 2010
  • Forum Post: Re: TVP7002 generating composite from RGBHV

    Larry Taylor Larry Taylor
    Hi Steve, Can you supply more detail on how the TVP7002>THS8200 evaluation board is being used? Which input and output formats are being used? Which dataset is being used to program the evalution board using the WinVcc EVM software?
    on Jun 21, 2010
  • Forum Post: Re: TVP7002 generating composite from RGBHV

    Steven Mattu Steven Mattu
    Hi Larry I have tried a composite to composite conversion using the evaluation board that worked fine. With that I connected an YCbCr signal to the BNC (TVP7002 side) of the evaluation and got a working YCbCr signal out from the THS8200 side. The resolution was at 720p and the preset I used...
    on Jun 21, 2010
  • Forum Post: Re: TVP7002 generating composite from RGBHV

    Larry Taylor Larry Taylor
    Steve, I am unable to reproduce this issue here using 720p+discrete syncs connected to the VGA connector on the EVM. On the TVP7002 Status Property Sheet: Is 750 lines reported in the Lines/frame status? Is "From HSYNC" and "From VSYNC" reported in the Sync Input Status...
    on Jun 21, 2010
  • Forum Post: Re: TVP7002 generating composite from RGBHV

    Steven Mattu Steven Mattu
    Hi Larry I have managed to solve the problem thanks to the questions you asked. The VSYNC was present on U6 and both syncs were present in the Sync Status Boxes. However, when I checked the lines/frames value it was 746 measured value on the TVP7002 and was 750 in the property sheet for the...
    on Jun 22, 2010
  • Forum Post: Re: TVP7002 generating composite from RGBHV

    Larry Taylor Larry Taylor
    Steve, Glad you figured it out. It looks like the RGB source may not be standard 720p. Larry
    on Jun 22, 2010
  • Blog Post: New Data Manual Releases

    Foe Foe
    New data manual releases are now available from ( http://www.ti.com/ ) for the following TVP devices. Part Number Literature Number Release Date TVP5146M2 SLES141G April 2011 TVP5147M1 SLES140F December 2010 TVP5150AM1 SLES209E October 2011 TVP5151 SLES241E October 2011 TVP5154A...
    on Jul 29, 2010
  • Blog Post: New Application Note Releases

    Foe Foe
    The following new TVP/THS application notes are now available from ( http://www.ti.com/ ). Literature Number Release Date Description SLEA073A August 2009 TVP5158 PCB Layout Guidelines SLEA075 September 2009 TVP5151 PCB Layout Guidelines SLEA076 June 2010 THS8134B PCB Layout Guidelines...
    on Jul 29, 2010
  • Forum Post: TVP700x Settings for RGB 4:4:4 Conversion with Sync on Green (SOG)?

    Bernie Thompson TI Bernie Thompson TI
    I am looking for some settings for a TVP7001 application where it needs to convert to RGB 4:4:4 from a camera providing: -Analog RGB -Interlaced -Sync on green -768x494 resolution Does anyone know of any example register settings that could be used to start with to get to this configuration (or...
    on Sep 2, 2010
  • Forum Post: Re: TVP700x Settings for RGB 4:4:4 Conversion with Sync on Green (SOG)?

    Larry Taylor Larry Taylor
    Bernie, Try the settings below for this format. It is not clear what the total pixels per line are for this format. The settings below are based on a camera found that specified 768 active and 811 total pixels/line. This may requrie adjustment for your camera. A 2x PLL setup with DIV/2 was used to...
    on Sep 2, 2010
  • Forum Post: Re: TVP700x Settings for RGB 4:4:4 Conversion with Sync on Green (SOG)?

    Bernie Thompson TI Bernie Thompson TI
    Thanks for the fast response, this sounds like it is just what I was looking for.
    on Sep 2, 2010
  • Forum Post: Re: TVP5150 non-standard video

    Logan West Logan West
    Thanks Larry, From what I can tell, the TVP7002 is for component video, and RS-343 is a Composite signal so unless I'm mistaken, I don't think this would work. I appreciate the help though.
    on Oct 5, 2010
  • Forum Post: Re: TVP5150 non-standard video

    Larry Taylor Larry Taylor
    Logan, Monochrome RS343 shouldn't have any color or chrominance present, so YC separation shouldn't be necessary. You should be able to treat it as the luminance (Y) component. If support for color composite video is requried, then a video decoder would be requried.
    on Oct 5, 2010
  • Forum Post: Re: TVP5150 non-standard video

    Logan West Logan West
    Larry, You are correct, I got ahead of myself there. Thanks for your help.
    on Oct 5, 2010
  • Forum Post: Re: TVP5146 Sync on Green Support?

    James Nave James Nave
    Tai, The TVP7002 video ADC supports VESA PC graphics formats; however, it does not support CVBS or S-Video. Regards, Jim
    on Nov 16, 2010
12345»
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use