• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Data Converters » Video Converters » All Tags » ths8134b
Share
Video Converters
  • Forum
  • Announcements

Browse by Tags

Video Converters

Welcome to the Video Converters Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
ths8134b
  • TFP401
  • THS8133B
  • ths8135
  • THS8136
  • ths8200
  • TVP5146M2
  • TVP5147M1
  • TVP5150AM1
  • TVP5151
  • TVP5154A
  • TVP5158
  • TVP5160
  • TVP7002
Related Posts
  • Blog Post: New Application Note Releases

    Foe Foe
    The following new TVP/THS application notes are now available from ( http://www.ti.com/ ). Literature Number Release Date Description SLEA073A August 2009 TVP5158 PCB Layout Guidelines SLEA075 September 2009 TVP5151 PCB Layout Guidelines SLEA076 June 2010 THS8134B PCB Layout Guidelines...
    on Jul 29, 2010
  • Forum Post: THS8134B

    Larry Blumer Larry Blumer
    Hi, I'm using a THS8134B to output an RGB VGA signal. I have tied M1, M2 to GND and SYNC# and SYNC_T to DVdd. What I am seeing is an offset (300-500mV) on the green output. I've tried a few things but the offset still remains. I have noticed that the 8135 or 6 would seem to have another mode...
    on Sep 8, 2010
  • Forum Post: Re: THS8134B

    Larry Taylor Larry Taylor
    Hi Larry, The THS8134B offset is apllied to the green channel to allow room for sync insertion and cannot be disabled. This is typically not an issue with video or graphics applications where the outputs are AC coupled prior to the monitor's DC restore. You are correct that with the THS8135...
    on Sep 9, 2010
  • Forum Post: Re: THS8134B

    Larry Blumer Larry Blumer
    Hi, Thanks for the resonse. I had tried to AC couple the green signal, I had used a 10nF cap, not quite sure waht value would be best. What I see when I do that is a violet tint. I suspect now I'm not getting enough green drive? Thanks, Larry
    on Sep 9, 2010
  • Forum Post: Re: THS8134B

    Larry Taylor Larry Taylor
    How does it look if you DC couple the green channel? 10nf is too small. The monitor should be able to handle a DC coupled input with the offset, since it problaby also supports sync-on green. Color inbalance could also occur if: - RGB mode is not enabled in the THS8134B. To ensure RGB mode, you...
    on Sep 9, 2010
  • Forum Post: Re: THS8134B

    Larry Blumer Larry Blumer
    Hi Larry, Thanks for the response. When I DC couple there is a green tint, this varies with the display used. I'm driving a Dell VGA monitor and another small display. The datasheet is a little unclear, I'm setup for RGB mode M1,M2 = GND Syncs = H. Currently I can't pulse the syncs...
    on Sep 9, 2010
  • Forum Post: Re: THS8134B

    Larry Taylor Larry Taylor
    Larry, Sounds like you have been careful with HSYNC position. HSYNC and VSYNC polarity, length, position are all important for digital monitor format detection and correct clamp or DC restore position. Are you using the /Blank control input to force blank or black level? If you look at RGB at...
    on Sep 9, 2010
  • Forum Post: Re: THS8134B

    saptarshi dutta saptarshi dutta
    Larry, Can i use the RGB output of tfp401 to drive the video DAC ths8134b.What will be the clock for DAC and how to get a seperate Sync from a embedded sync on green/sync on all channels. Saptarshi
    on Feb 18, 2011
  • Forum Post: video converters

    saptarshi dutta saptarshi dutta
    I am thinking of following choices: converting a HDMI signal to a DVI -------------via a cable Using a DVI receiver-------------------------------TFP401 Taking the 24-bit RGB output and connnecting the same to a video DAC THS8134B. Connecting this analog RGB/YPbPr output from DAC to a...
    on Feb 18, 2011
  • Forum Post: Re: video converters

    Larry Taylor Larry Taylor
    Saptarshi, The TFP401 can output 1 pixel/clock over 24 bits, instead of even/odd. To connect to a DAC, single pixel 24-bit should be used. One potential issue with this is an 8-pixel latency through the DACs. Analog RGB out will be delayed relative HS. HS will have to be delayed somewhere in the...
    on Feb 18, 2011
  • Forum Post: Re: THS8134B

    Larry Taylor Larry Taylor
    Saptarshi, See post at http://e2e.ti.com/support/data_converters/videoconverters/f/376/p/94683/330049.aspx#330049
    on Feb 18, 2011
  • Forum Post: Re: video converters

    saptarshi dutta saptarshi dutta
    Thanks Larry I think i will have to operate TFP401 in 1pixel/clock mode instead of 2pixel/clock. How the HS be delayed using I2C control?? Tell me which video DAC i need to use (THS8135 or THS8134B or THS8200) keeping in mind that TFP401 gives out 24 bits of RGB. (so probably 8 bit...
    on Feb 21, 2011
  • Forum Post: LCD to RGsB on low resolutions?

    Aleksey Susik Aleksey Susik
    Hello, I need to convert digital LCD signal to analog RGsB using ths8134b. But I think there will be a problem with low screen resolution (320x240 or so). Is it possible to make this video dac to work with 5-6MHz pixel clock? Thank you!
    on Mar 6, 2011
  • Forum Post: Re: LCD to RGsB on low resolutions?

    Larry Taylor Larry Taylor
    Hi Aleksey, The THS8134B should work fine at these lower pixel rates.
    on Mar 7, 2011
  • Forum Post: THS8134B

    Stefano54155 Stefano54155
    Hi, I'm using a THS8134b to get an RGB VGA output from a BT.656 1x8 bit input. I have tied M1, M2, /SYNC, SYNC_T and /BLANK to 3.3V and I am using GY7..0 as data input. Unconnected pins 9, 10, 13, 14, 35, 36 are tied to ground. Input data are coming from a DM365 in BT.656 standard with a...
    on Sep 1, 2011
  • Forum Post: Re: THS8134B

    Larry Taylor Larry Taylor
    Hi, If you are trying to convert 8-bit YCbCr to RGB, the THS8134B cannot support this. You will need a device with a color space converter, such as the THS8200. Note that when an 8-bit interface is used with the THS8200, digital embedded syncs must be used.
    on Sep 1, 2011
  • Forum Post: Re: THS8134B

    Yucheng Yucheng
    Hi, Same question. I used YCbCr-out to THS8134/5, but cannot convert data... the document show can do it. why cannot do it ?
    on Sep 16, 2011
  • Forum Post: Re: THS8134B

    Larry Taylor Larry Taylor
    The THS8134/5 can support both RGBin/RGBout and YCbCr in/ YPbPr formats, but it cannot convert between RGB and YPbPr. The digital coding for the two color spaces are different. A color space converter is needed to convert color spaces. The RGB<>YPbPr mode switch in the THS8134/5 just changes the...
    on Sep 16, 2011
  • Forum Post: Re: THS8134B

    Yucheng Yucheng
    Hi, Does THS8134/5 supports ITU-BT.656 input mode ? YCbCr 8bit input --> YPbPr outbut ?
    on Sep 19, 2011
  • Forum Post: THS8134B convert YCbCr

    Yucheng Yucheng
    Hi, How do convert YCbCr BT656 8bit video source? DM36x YCbCr out (BT656) --> THS8134 YPbPr out.
    on Sep 23, 2011
  • Forum Post: Re: THS8134B convert YCbCr

    Larry Taylor Larry Taylor
    Hi Yucheng, The THS8134B does not support bt656 with embedded digital syncs. For bt656 support with embedded sync support see the THS8200.
    on Sep 24, 2011
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use