Hi,
I'm trying to use a ccs project but it says you need to install c2000 v6.1 compiler . I have c2000 v6.0.1 and I don't see anything about c2000 while checking for updates. Can you show me how to download it?
Hi Ismail,
please send me a friend request and I can send you the compiler version offline.
Best Regards,Lisa
Hi Lisa,
Apart from compiler problem (I'm waiting to get it from you),
I've had Example_2806xSci_Echoback worked. I want to make it work also in phy_tx_rx_vcu of plc phy example. But when I add files of echoback to phy_tx_rx_vcu and initialize system control it gives compilation error. What am I supposed to do?
line 141: error #148: declaration is incompatible with "void InitSysCtrl(void)"
Hi again,
I've just made a simple mistake of not putting that command in the main function. Sorry about that. Still waiting for the compiler.
I received your friend request and am in the process of setting up the download link for you, so don't worry. As soon as it is setup I will send you an offline note with instructions.
Best Regards,
Lisa