I am starting to work with 28035 Experimenter Kit. First thing was following steps on System Framework Overview pdf file and could get FlashingLed example running without problems.
Checked example results and closed CCS4 when finished working.
Next time I tried to run Flashing Leds example, I opened CCS4 on the corresponding workspace.
Tied to connect to Target hitting debug button but cannot connect to Target, and I get the error message:
Error connecting to the target:Error 0x80000200/-1142Fatal Error during: OCS, Processor blocked debug accesses. An operation was attempted whilethe CPU was in a non-debuggable context. To continue to honor the debugcontext, press Cancel. To force debug access, press Rude Retry.
tried several times checking Debuggging configuration with no success
After checking some other answers in this forum, I understand this problem might be related with Real Time Mode debugging but could not get the Target running again. Always getting same message.
Look forward to getting an answer which helps me get this going.
Thanks
Daniel,I would recommend making sure that your version of CCS is up-to-date. I remember having this issue during some earlier release (if I remember correctly, the issue is the real-time mode is getting stuck being on). The latest version of CCS4 is 4.2.5You can usually update CCS from within CCS. (Help->Software Updates->Find and Install...)---If you desire, you can also just directly download the most recent version. Both CCS4 and CCS5 are both currently supported (although new releases are only being planned around CCS5). Both can be downloaded from the below link:http://processors.wiki.ti.com/index.php/Download_CCSThank you,Brett
Hi Brett,
Thanks for your input.
CCS version I was using was 4.2.1. I uninstalled it and intalled CCS from the DVD I got with Experimenter Kit.
Now CSS version is 4.2.3.00004. I got new license and everyting seems to be working Ok.
I tried then to run Flashing LEDs example. First deleted old workspace files and created new workspace just following directions from "SystemFrameworkOverview" pdf file.
Rebuilt project with no errors. When launching the debugger I don´t get expected debugger window status. Nevertheless I try to get target running but get this error message:
Trouble Reading PC Register:(Error -1142 @ 0x0)Device blocked debug access because it is currently executing non-debuggable code. Choose 'Rude Retry' to disable polite mode and force the operation.(Release 5.0.333.0)
If I choose Rude Retry, it seems that target starts running but variable Gui_LedPrd_ms value is 24382 and doesn¨t change in spite of selecting permanent refresh in Watch window.
Seems that the target is caught in an odd status and I can´t get it out of it? May be CLA status?
Any hints will be very much appreciated.
Regards
Daniel
Hi again Brett,
New Findings: If I starrt debug session hitting debug button I get all the problems I mentioned.
If first I "Launch TI Debugger", then "Connect Target", then "Load Program" and select FlashingLeds... RAM.out, program is loaded and everything goes smooth as expected.
I can change Gui_LedPrd_ms value and Led modifies blinking period, and I can stop the program and start it again.
With restart it goes to main line, etc.
Is any selected DEbug option misconfigured perhaps?
Thanks again for your input.
Daniel,FYI, v4.2.3 still isn't up-to-date, 4.2.5 is the most recent. I would still recommend updating to the most recent and you should be able to further update CCS from within CCS. (Help->Software Updates->Find and Install...). However, I no longer think this is your issue directly.Within CCS, go to Target->Debug... Here you should be able to see your settings for a "Non-Project Debug Session" and your "Project Debug Session". Based on what you're saying the settings for Non-Project Debug are correct and the Project Debug is wrong. See if you can change the project debug session to make both sessions' settings identical. I think the inconsistency would be under "Project Debug Session->Target->Generic Debugger Options->Realtime Options" Let me know if this still doesn't fix things. If it doesn't I think I'll need to pass you onto the CCS guys. (their first recommendation will be to update CCS though :))Thank you,Brett
Brett,
Thanks for your answer.
Following your input I updated CCS to version 4.2.5. But as you aniticipated, problem was still there.
I checked realtime option for both Non-Debug and Project Debug Session, without any success.
Then I checked other configuration differences between Non- Debug and Project Debug Session.
I found that for Project Debug Session, under Common, Shared file option was selected with a Flashingled....out file selected in the corresponding window.
As in NonDebug Session, Local File option was selected, I changed Porject Debug Session configuration to Local File also.
This seems to get things working OK. But I don´t really understand the difference.
Can you please explain briefly what changes with Local File/ Shared File selection?
Thanks for your support
Daniel,
I'm not really sure. CCS is not my forte, but I'm usually able to get things going. My guess is that somehow the project's CCS workspace got corrupted in your earliest port to the older CCS. I have a suspicion that if you created a new workspace that things would work first pass from CCS 4.2.5.I'll move this post to the CCS forum to see if they have any input.Thank you,Brett
Hi Daniel,
Daniel Alba I found that for Project Debug Session, under Common, Shared file option was selected with a Flashingled....out file selected in the corresponding window. As in NonDebug Session, Local File option was selected, I changed Porject Debug Session configuration to Local File also. This seems to get things working OK. But I don´t really understand the difference. Can you please explain briefly what changes with Local File/ Shared File selection?
the difference between the two is where the launch configuration for the project is stored. When selecting 'Local', it is managed by CCS, hidden, and stored in the workspace metadata folder. When selecting 'Shared', it is stored in the project folder and accessible. It is considered 'Shared' because this folder can then be checked into source control and shared with others.
What I am not sure of is how it had an impact on your actual debug session. I suspect that there was something messed up with your launch configuration and changing the settings cleared it (one of our tips and tricks to resolve strange CCS debug issues is to delete you old cached launch configurations).
ki
-----------------------------------
Don't forget to verify answers to your forum questions by using the green "Verify Answer" button.
Did you read the CCS Forum Guidelines & FAQ? If not, PLEASE read it. If you haven't read it in awhile, please read it again to see if any updates were made.
Having CCSv5 problems? Check out the CCSv5 Troubleshooting Guide
Click here to track an issue. Enter your bug id in the "Find Record ID" box
Thanks for your answer Ki.
Regards,