I just installed CCSv5.2.1.00018 on Ubuntu 12.04 32-bit. I would like to connect to OMAP-L137 EVM. When I create a new Target configuration, there are no boards or devices listed under "Spectrum Digital DSK-EVM PLUS onboard USB Emulator", so I dusted off the XDS100v2, and select OMAPL137 device. I ask for Test Connection, and all is reported OK. I go to debug session, and I get this error message:
Error connecting to the target:(Error -1063 @ 0x0)Device ID is not recognized or is not supported by driver. Confirm device and emulator configuration is correct, or update device driver.(Emulation package 5.0.747.0)
If instead I select c6747 device, connection is OK.
Am i missing something from my install, or is L137 a lonely orphan?
Hi,
Per your description it seems you have a XDS100v1 emulator, which only supports C674x devices (the DSP-side of OMAPL137).
I managed to reproduce the exact same scenario as yours (test connection ok, fails to connect to ARM9) - in my case I am using a XDS100v1 emulator but configured it as a XDS100v2 on the Target Configuration Editor.
Therefore, to be able to connect to the ARM9 core you will need a XDS100v2 emulator.
Regards,
Rafael