Using PSP with Code Composer Studio 4

Hi,

I have a working project with C642x based on PSP_1_10_03, NDK2.0 and Code Composer 3.3.

It was a hard work to put it all together, but I have to thank TI because it saves me a lot of month of work: I think without these softwares the time-ratio is more than 10:1...

Now I see the new CCS4, and I am interested to port my project to it.

I have a lot of problem to understand how the tree structure of PSP_1_10_03 work with the workspace structure of CCS4. Using the "Import Legacy CCSv3.3 Project" tool with this complex structured project is far from easy, at least for me...

Do you know if is planned a new PSP revision for CCS4? If not there's a wiki/tutorial to use PSP with CCS4?

Best Regards,

Alberto