• Resolved

CCS: Error in CCS Version

Tool/software: Code Composer Studio

I have created a new project in CCS using already existing source files. I am facing following error : 

Severity and Description Path Resource Location Creation Time Id
file "../Source/2806x_BootROM_API_TABLE_Symbols_fpu32.lib<TMS320x2806x_boot_rom_out___romApi_Flash2806x_DepRecover_tmp.obj>" specifies ISA revision "C28FPU32", which is not compatible with ISA revision "C2800" specified in a previous file or on the command line ver4 line 0 1488195658759 241

I also have CCS 7 installed on my system.Please help me with the error.

  • Guru 140050 points

    Please see this FAQ at this link.


    Please click This Resolved My Issue if the reply answers your question.

    Search the wikis for common questions: Compiler, CCSv6, CCSv7
    Track a known bug with SDOWP. Enter the bug id in the "Find Record ID" box