TMS470MF04207: TMS470MF04207: Simultaneous Flash Operations on multiple JTAG probes

Part Number: TMS470MF04207

Hello,

My question is fairly simple:

Is it possible to use several JTAG probes (XDS100V2) connected to the same PC to perform flash operations on several TMS at the same time using uniflash (version does not matter) ?

I remember that on NowFlash, there was a possibility to select a port, I wonder if this the JTAG probe's port and if it is, if there is a similar option in uniflash.

Anyway, I could not find an option like that in uniflash 3, 3.4, and 4.

Thank you !

Kind regards,

Christophe Bonniot