This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

CCS: SimpleLink™ CC2650 project 0 does cot compile any more on the cloud CCS

Tool/software: Code Composer Studio

Hi

I have imported the SimpleLink™ CC2650 project 0 in my CCS workspace a year agao. Compilation and build were ok last week. But  it fails now

The two projects are
ProjectZeroApp_CC2650LAUNCHXL
ProjectZeroStack_CC2650LAUNCHXL
here are the first few erros
========================

>> Compilation failure gmake[1]: Leaving directory `@ti-rex-content/simplelink/ble_cc26xx_2_01_00_44423_cloud/Projects/ble/ProjectZero/CC26xx/CCS/Config/src/sysbios' Build of libraries failed. TOOLS/subdir_rules.mk:10: recipe for target 'build-1577816961-inproc' failed

error: symbol "xdc_runtime_System_printf_va__F" redeclared with incompatible type: "xdc_Int(xdc_CString, va_list)[int [ExplSign] ]" in "@ti-rex-content/xdctools_3_31_01_ 33_core/packages/xdc/runtime/System.h" at line 285 and: "Int(CString, VaList)[xdc_Int [int [ExplSign] ]]" in "/Tirex_Content/testing0/xdctools_3_31_01_33_core/packages/xdc/runtime/Syste m.c" at line 243)

error: symbol "xdc_runtime_System_aprintf_va__F" redeclared with incompatible type: "xdc_Int(xdc_CString, va_list)[int [ExplSign] ]" in "@ti-rex-content/xdctools_3_31_01_ 33_core/packages/xdc/runtime/System.h" at line 294 and: "Int(CString, VaList)[xdc_Int [int [ExplSign] ]]" in "/Tirex_Content/testing0/xdctools_3_31_01_33_core/packages/xdc/runtime/Syste

...
==========================
Your help is really appreciated. Thanks in advance.
Rgds
Jidong
  • Guru 146330 points

    Jidong,

    As per this post, the CC2650 SDK is no longer enabled in CCS Cloud.

    You can still download the SDK from here, install desktop CCS (download from here) and import and build projects using the desktop CCS.

    ____________________________________________________________________________

    Please click This Resolved My Issue if the reply answers your question.

    Search the wikis for common questions: Compiler, CCSv6, CCSv7
    Track a known bug with SDOWP. Enter the bug id in the "Find Record ID" box

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.