CCS/TMS320F28377D: Issue with loading program on to CPU2

Part Number: TMS320F28377D

Tool/software: Code Composer Studio

I am using Texas Instruments XDS100v2 USB Debug Probe to program the TMS320F28377D microcontroller and I am facing some problems while trying to program CPU02. It says

"C28xx_CPU2: File Loader: Verification failed: Values at address 0x08000@Program do not match Please verify target memory and memory map.

C28xx_CPU2: GEL: File: 'xxx'.out: a data verification error occurred, file load failed."

Earlier I was just programming the RAM and I didn't had any issue, but recently I tried to program the CPU2 flash and that's when I started having these problems. Now, even when I try to just program the RAM, it doesn't allow me and this error keeps popping up. 

Did I mess something while trying to program the Flash?

P.S. I  am using CCS Version: 7.4.0.00015 and I also tried to flash the CPU2 with UniFlash, but it also throws the same error "[ERROR] C28xx_CPU2: File Loader: Verification failed: Values at address 0x08000@Program do not match Please verify target memory and memory map."

5 Replies

  • Hello,
    Are you trying to load an example from controlSUITE/C2000Ware or is this a custom program? If it is the former, please let me know which example. If it is the latter, can you provide a test case?

    Thanks
    ki

    -----------------------------------

    Did you read the CCS Forum Guidelines & FAQ? If not, PLEASE read it. If you haven't read it in awhile, please read it again to see if any updates were made.

    Having CCS problems? Check out the CCS Troubleshooting Guide

    Looking for CCS Training? Check out the CCS Training Site

    Curious about the status of a bug and know the tracking ID? Track it via the public bug tracking portal

    NOTE: When a bug is filed and a tracking ID is provided, the thread may then be suggested as "TI Thinks Resolved". Why? Please read the first FAQ of the CCS Forum Guidelines & FAQ

  • In reply to Ki-Soo Lee:

    Hi,

    I am trying to load a custom program, but I also tried the example blinky_dc from the controlSUITE. I had the same error with both of them.

    Best Regards,
    Sai
  • You are getting a verification error at 0x8000. That is RAM. But you mentioned that the issue occurs when programming Flash.

    I tried the blinky_dc example with CCSv7.4.0. There were no issues loading/flashing.

    Can you tell me step by step what you did to reproduce the issue with the blinky_dc example? 

    Thanks

    ki

    -----------------------------------

    Did you read the CCS Forum Guidelines & FAQ? If not, PLEASE read it. If you haven't read it in awhile, please read it again to see if any updates were made.

    Having CCS problems? Check out the CCS Troubleshooting Guide

    Looking for CCS Training? Check out the CCS Training Site

    Curious about the status of a bug and know the tracking ID? Track it via the public bug tracking portal

    NOTE: When a bug is filed and a tracking ID is provided, the thread may then be suggested as "TI Thinks Resolved". Why? Please read the first FAQ of the CCS Forum Guidelines & FAQ

  • In reply to Ki-Soo Lee:

    I also didn't had any issue running the blinky_dc example earlier. But now it is throwing the data verification error. The timeline of the events is as follows.

    Till yesterday afternoon everything is fine. I am running my custom program on both the CPUs and they were working fine. I made some changes to the CPU2 code and tried to reprogram the RAM. The flash was successful, but I didn't see any change in the code. (I tried it 2-3 times and since there was no change, I purposefully modified a return statement from a meaningful value to 0. It continued to return the meaningful value instead of 0). So, I changed the project configuration from CPU2_RAM to CPU2_FLASH. I built the project and entered the debug mode. It threw a bunch of errors (something like CPU1 is not defined and so on) and the load failed. I changed the project configuration back to RAM and again rebuilt the program. Now, I opened the UniFlash and selected the option "Erase Flash" in Settings and Utilities section of CPU2. Then I tried to load the .out file through UniFLash and it threw the data verification error. I tried it with CSS, but I had the same error again.


    Later, I imported the blinky_dc example into my workspace and ran the Code Composer Debug Session. But, it also had the same error while loading the .out file.
  • In reply to Sai Madem83:

    For CPU2, if you open the Memory Browser view and specify to view Program Memory at 0x8000, Are you able to edit the contents of memory?

    -----------------------------------

    Did you read the CCS Forum Guidelines & FAQ? If not, PLEASE read it. If you haven't read it in awhile, please read it again to see if any updates were made.

    Having CCS problems? Check out the CCS Troubleshooting Guide

    Looking for CCS Training? Check out the CCS Training Site

    Curious about the status of a bug and know the tracking ID? Track it via the public bug tracking portal

    NOTE: When a bug is filed and a tracking ID is provided, the thread may then be suggested as "TI Thinks Resolved". Why? Please read the first FAQ of the CCS Forum Guidelines & FAQ