I am trying to install active perl and inline-java as per the steps mentioned in http://processors.wiki.ti.com/index.php/DSS_from_Perl.
But the link that the wiki shows for inline-java does not work and tried even other repositories to get the ppd package of inline-java.
Can anybody provide their inputs on how to install inline-java on windows machine either through perl package manger (activePerl version 5.10.*) or via compilation.
I have tried compiling the inline-java module using nmake on windows but no luck.
It throws the following error
Can't find string terminator "}" anywhere before EOF at -e line 1.NMAKE : fatal error U1077: 'C:\WINDOWS\system32\cmd.exe' : return code '0xff'Stop.
Any instructions on how to install the inline-java would be really helpful.
Thanks in advance,
Murali.
If the command line install is failing, try running the ppm GUI.
Go to 'Edit->Preferences->Repositories' and add the path to the repository:
Then you should see the Inline-Java package available:
-----------------------------------
Don't forget to verify answers to your forum questions by using the green "Verify Answer" button.
Did you read the CCS Forum Guidelines & FAQ? If not, PLEASE read it. If you haven't read it in awhile, please read it again to see if any updates were made.
Having CCSv5 problems? Check out the CCSv5 Troubleshooting Guide
Click here to track an issue. Enter your bug id in the "Find Record ID" box
Hi,
My problem is when i try to download using PPM manager it gave a message
Downloading ActiveState Package Repository packlist ... failed 500 Can't connect to ppm4.activestate.com:80 (Bad hostname)
when i tied to do the above mentioned step , there is a similar error message
Downloading UWIN packlist ... failed 500 Can't connect to cpan.uwinnipeg.ca:80 (Bad hostname)
I am not sure on what is the exact issue .
Do some one having some idea ?
Thanks in advance
sasi
Hi sasi,
It could just be an issue of the server being down. You can try downloading the whole package manually and install it offline.
Thanks
ki
thanks ki,
But when i tried to run the downloaded version and install using
ppm install inline_java12\inline_java the error is
ppm install failed : The ppd does not provide code to install for the platform
Do you know what have to be done for this ?
Regards