Can anyone provide a description of what an OTIS error might be? I am asking on the Code Composer Studio forum because we went through a lot of trouble to get older emulator drivers and CC drivers that were reported to be compatible with our older 'F206 (aka c2xx or c24x) DSP. I am wondering if this is could be an error related to newer device support that is documented in another manual for support for any newer DSP.
We are using a prg2xx.exe command line utility with an SPI525 emulator pod to program a TMS320F206. We have some boards that give Error 103 (memory) errors, but we also are seeing "OTIS Error -1" errors that are not documented in the old TI readme PDF that we are referencing (TMX320F2XX JTAG Based Flash Programmer, Revision 2.0, 09/22/97) .