I am trying to make the MSP430BT5190-CC2560 SDK to the MPS430 experiment board. However, there are fetal errors when I make the accl and temp under the SPP. The errors are all saying it could not open some source file.
Like this:
Fatal Error[Pe005]: could not open source file "sdk_pl.h" C:\MSP430BT5190-CC2560 SDK\Beta 1.0\MSP430- CC2560_Applications\Source\bluetooth\export\accl_appl\accelerometer_pl.c 11
searched: "C:\MSP430BT5190-CC2560 SDK\Beta 1.0\MSP430-CC2560_Applications\Source\bluetooth\export\accl_appl\"
searched: "C:\Program Files\IAR Systems\Embedded Workbench 5.4 Evaluation\430\INC\"
searched: "C:\Program Files\IAR Systems\Embedded Workbench 5.4 Evaluation\430\INC\DLIB\"
It seems that the file "sdk_pl.h" is in the "C:\MSP430BT5190-CC2560 SDK\Beta 1.0\MSP430-CC2560_Applications\Source\bluetooth\private\accl_appl\" which is not in the searching area.
How can I solve this problem?
Thanks.
Sylvia