I had been running CCS version 3 on my MacBook Air under Parallels without any difficulty. Actually due to the solid state memory it was very much faster than on my previous Dell. Windows7 is installed via BootCamp and runs concurrently with Parallels. I had no trouble both building and debugging. I'm using a MSP-FET430UIF-VCP ICE to connect to my development board. Recently, because we are now using an MSP430F5528 we upgraded to CCS 4.2.3. Building continued to work fine but I could no longer debug as CCS would complain that the target device was not connected. I know the ICE is in fact connected as I can see it listed under Windows7. My work around has been to use BootCamp and boot up into Windows7 and run native. Although this works I would much rather run CCS under Parallels so I can concurrently have access to all my other Mac services - email, etc.
Has anyone else run in a similar setup with success?
Dick