This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Here the screenshot from SD's SDConfigEx tool:
Hi Andre,
it looks like the emulator is pointed to or trying to use the wrong driver.
Please get the 64 bit drivers for CCSv5 here and try installing them and try again.
http://www.blackhawk-dsp.com/support/Drivers.aspx
Please keep us posted.
Best Regards,
Lisa
Andre,
There is a chance this emulator is not supported in Windows 7/64. According to the XDS510PP+ page at the Spectrum Digital's website, the list of operating systems supported does not show Win7.
I will check with Spectrum Digital to confirm that. I couldn't make the emulator work in my system here as well, but I get a different error message from SdConfig that may have other causes.
Regards,
Rafael
HI Andre,
unfortunately Rafael and I have been able to confirm the parallel port is not supported under 64 bit windows or linux. This comes directly from spectrum digital. Sorry for any inconvenience.
Best Regards,
Lisa
Lisa TI said:Hi again Andre,
I meant to point you to the spectrum digital site for the drivers ...
http://emulators.spectrumdigital.com/
Best Regards,
Lisa
I also had this idea, but as you can see, there are only drivers until CCS v3.1: http://emulators.spectrumdigital.com/c2000/
According to Spectrum Digital, newer CCS versions already have a driver integrated, so obviously there is no need for them to publish a new one. This can be read right there: http://support.spectrumdigital.com/ccs40/ (first paragraph, in Step 1: "All Spectrum Digital JTAG emulation drivers and CCStudio target configurations for the CCStudio v4.x platform are included with the Code Composer Studion software installation.").
This is quite bad news. But anyway, thanks for your answers.Lisa TI said:HI Andre,
unfortunately Rafael and I have been able to confirm the parallel port is not supported under 64 bit windows or linux. This comes directly from spectrum digital. Sorry for any inconvenience.
Best Regards,
Lisa
Does anyone have experiences with a parallel port pass through from virtual machines like VMware or Virtualbox? The idea is to install one of these virtualization solutions on the new Win7 computer and pass through the parallel port to an virtualized Windows XP - so we would be able to use this old environment for some legacy projects. Any experiences on this?
HI Andre,
we have tried through a XP VM setup and unfortuantely could not pipe the emulator through. Unfortunately I suspect the host may need to have driver support to pass the device into the VM.
Sorry for the bad news.
Best Regards,
Lisa
Thanks for your efforts. Which virtualization solution do you have tested? The XP mode from Win7 (based on MS's Virtual PC 2007) doesn't seem to support parallel port pass-through, but at least with VMware Player 4.0.1 build-528992 I am able to add a virtual parallel port to a VM which has the option to use a physical parallel port on the host. This looks promising.
Hopefully I will have time to test this in the near future.
Andre,
Have you been able to get the XDS510PP_Plus emulator to work with Win7 be using the VMWare Player? We have the same issue and are unhappy about switching to other emulators, as they don't work nearly as well as the XDS510PP_Plus and they cost a whole lot more.
Nelson
I'm sorry, but I didn't had the time for testing this. But if this problem here will be getting hotter (read: if we run out of Windows XP computers), I will try this.
No, we couldn't find a real solution. We just keep two old laptops with Windows XP running for the sole purpose of using this debugger.