Hi,
I've read this wiki link http://processors.wiki.ti.com/index.php/Projects_-_Command_Line_Build/Create for getting information about building a project from the command line. Using this command:
eclipsec -nosplash -data v:\CCSv5_Workspaces\mainLine -application com.ti.ccstudio.apps.projectBuild -ccs.projects DTecSensorDsp -ccs.buildType full
It works well until a first warning message is displayed from the compiler, then the process hangs and it won't continue. For example, this is the last message displayed after having several files successfully compiled:
'Building file: V:/Perforce/software/embed/mainLine/M_EMB0006_drivers/src/dm6437/i2c.c'
'Invoking: C6000 Compiler'
"C:/CCSv5/ccsv5/tools/compiler/c6000/bin/cl6x" --cmd_file="V:/Perforce/software/embed/mainLine/M_EMB0003_dtec/proj/CCSv5/dtecMain/Cfg/includePaths.opt" -mv64+ -g -O2 --gcc --define=_NO_IR_CUT_FILTER
--define=PN_53A0010 --define=TRACKING_ALGO_TEST_VECTOR_ENABLE --define=DEVICE_TYPE_DTEC --define=USE_CUSTOM_DATA_SERVER --define=LEGACY_EEPROM_SUPPORT --include_path="C:/CCSv5/ccsv5/tools/compiler/c60
00/include" --include_path="C:/CCSv5/ccsv5/../bios_5_41_11_38/packages/ti/bios/include" --display_error_number --diag_warning=225 --abi=coffabi --preproc_with_compile --preproc_dependency="src/M_EMB00
06_drivers/dm6437/i2c.pp" --obj_directory="src/M_EMB0006_drivers/dm6437" --cmd_file="./configPkg/compiler.opt" "V:/Perforce/software/embed/mainLine/M_EMB0006_drivers/src/dm6437/i2c.c"
"V:/Perforce/software/embed/mainLine/M_EMB0006_drivers/src/dm6437/i2c.c", line 529: warning #179-D: function "I2C_EnableFreeMode" was declared but never referenced
How can I make the process finish? Also, is there some documentation about additional options that we can specify on the command line (for example, if I want to send the output in a log file, etc.)
Thanks
Franck