Hi
I am trying to determine if I can still port single byte arithmetic from an existing software project
to the TMS320x code base. I notice the Code Composer Complier doesn't support single byte
variable type. An unsigned char is a word (2 bytes) long. Is there a work around, maybe a pre-compiler
or complier option to force char as a single byte in RAM allocation?
Thx
DC