I am using CCS V5 to develope code on the LM4F232H5QD EKS.
I was using CCS V5 yesterday without issue. Starting today it has become unstable. It is closing randomly when starting a debug session, stopping a debug session. Also without change to code, my one interrupt was not hitting a breakpoint during one session and on the very next session it was hitting.
I am developing a library and have a main program that serves as its functional test. I am having trouble duplicating when this happens, but it is happening frequently, every several minutes.
Is there a problem with starting to debug the functional test, stepping into a library or hitting a breakpoint in a library, then continuing?
I almost suspect that if I end the debug session while stopped in the library, the CCS project focus is set to the library. Then, if I am not attentive, I start a new debug session, but the focus is on the library, so CCS tries to load the library bare and that is when CCS exits unceremoniously. (just confirmed this happens.)
Any ideas? I am tired of restarting CSS every few minutes.
Regardless, CCS shouldn't just exit.
John