Hi TI Community,
I just started with my brand new C6A8168 EVM + with 8 GB SD Card (Linux Kernel 2.6.37) and the EVM came with a display device(a portable DVI connected LCD display). I'm using CCSv5.2 to program/debug. I'm using XDS100v2 JTAG connector.
What I would like to do is to display "Hello World" on the portable display.
The problem I'm facing is this:
1. (Before I added the GEL File to Target Configuration)
Error connecting to the target: (Error -1180 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 5.0.635.0)
-
2. (After I added the GEL File to target configuration evm816x.gel)
Error connecting to the target: (Error -1180 @ 0x0) Device is held in reset. Take the device out of reset, and retry the operation. (Emulation package 5.0.635.0)
Any help will be greatly appreciated.
Regards
Vikram