My licensed CCS studio single user software license expired ! Never understood that it could.
pls advice
/Henk mail : henk@can-west.nl
Hi Henk,
what type of license do you have? I assume a purchased full node locked? When did you get your license? Could you send a bit more details? If you send a friend/conversation request you can feel free to send the file itself for a look.
Best Regards,Lisa
Thanks Lisa for your prompt response !
I will mail you the details and thanks again as I finally found some time to use CCS in a new project.
/Henk
hi Lisa,
Noticed that I don't have your mail address.
Product is: CCSSUB TMDSCCSSUB-MCUN01-W , which was licenced on 1-21-2010 and expired on 1-21-2011. (just noticed it yesterday, as I never had time to use this product and was not aware that it would expire?)
note: At the same license date a second CCS product was licensed, but I don't quite understand the difference ?
TI Part design description: Code Composer Studio IDE - Microcontroller- Node Locked Single User (N01)
TI Part number : TMDSCCS-MCUN01-v4.0
pls advice and I hope you have a solution for me, as I just now will have to use this product !
thanks,
HI Henk,
you can simply send me a friend or conversation request with the license file for us to look at.
What exact message are you getting in CCS? How do you have CCS configured? Do I understand you found two license files? Which is CCS pointing to?
The above part number sounds correct. This is a full microcontroller node locked license for v4. Is this what you purchased? Note if you are trying v5, this is not a v5 license. So I assume you are using CCSv4? Is this correct?
Any further details would help us sort this out.
This is what is listed in my Regitered software:L
CCSTUDIO TMDSCCS-MCUN01-v4.0
Code Composer Studio IDE - Microcontroller - Node Locked Single User (N01) 01/21/2010 Active 9F54-9CC0-A3EE-11DE-B147-D52A-D455-B7B4
Primary: 00.1F.3A.7D.CE.82 Not Used 9F4F-1E80-A3EE-11DE-B147-F935-5E22-0DD3
CCSSUB TMDSCCSSUB-MCUN01-W SUBSCRIPTION - Code Composer Studio IDE - Microcontroller - Node Locked Single User (N01) 01/21/2010 01/21/2011 Expired! Active 9F78-EDA0-A3EE-11DE-B147-EA0B-E79C-9927
Primary: ANY - 9F4F-1E80-A3EE-11DE-B147-F935-5E22-0DD3
Hope this can solve the issue.
regards,
ok, I think it is your subscription, not your license that is expired.
When you run CCS, can you please confirm that you do no see unlicensed?
A subscription is what allows major upgrades (if with an active subscription you could migrate to a v5 license for example).
A CCS license itself never expires.
Hope this helps.
Best Regards,LIsa
dear Lisa,
As it askes me to register again,cannot use it at all. Problems with the lic file I suppose as the license cannot expire? Tried to find the lic file but cannot locate it. ( must have lost it after trouble with my computer? )
As I use my existing license file it is rejected, because it has been used allready.
Hope you can assist me in generating a new liv file, as I must have lost it !
Thanks again for your help and wait for advice,
if you lost your .lic file, unfortunately I will have to direct you to the license team at ccs_subscriptions@list.ti.com
As I said, a node locked license does not expire. A subscription can and that is what your message shows as expiring.
Thanks Lisa,
I recieved Henk's email request and hopefully I can help him from here.
Best Regards,
Sharon
Thank you very much Sharon!
Lisa