when I try to build model in Simulink for the C6713DSK board it gives the error below.
Error using ==> LinkCCS at 28
Error while connecting to Code Composer Studio(tm):
Error using ==> cu_compareAndWarnCCSVersions at 53
This version of the Embedded IDE Link CC does not support your
version of Code Composer Studio(TM) IDE.
The Code Composer Studio(TM) version supported in this release is 3.3.
Refer to the Embedded IDE Link CC data sheet
for more information on product requirements.
My DSK c6713 came with CCS v3.1. I have got the CCS v3.3 with me as well.
Can I install both or do I have to uninstall v3.1 before installing v3.3?
If I have to uninstall v3.1 can I still use the flash burn 2.8, drivers and target
content which came along with the board?
Thanks,
Shash