hi
I`m work with tms6437 and i have a faced with error when i load a program into it :
Trouble Writing Register: Error 0x00000006/-1176 Error during: Memory, Register, The IM memory request is not serviced by the HW memory system. This could be caused by the memory address specified does not exist in the specified memory/cache level. Sequence ID: 6 Error Code: -1176 Error Class: 0x00000006
I disable two deafalt breakpoint too.but it wasn`t changed.
please help me
thanks