Hello,
Stefano Sartorelli All cores can be loaded but core2 which is failing with the error: Error loading "../core2/Debug/Core2.out": File: /core2/Debug/Core2.out: a data verification error occurred, file load failed.
Are you loading the same program on all the cores and only core 2 fails? Are you using any GEL startup files with your target configuration?
Note the gotcha regarding the emulator drivers when installing on Linux. Did you install as root?
http://processors.wiki.ti.com/index.php/Linux_Host_Support#Ubuntu_12.04_64bit
Thanks
ki
-----------------------------------
Don't forget to verify answers to your forum questions by using the green "Verify Answer" button.
Did you read the CCS Forum Guidelines & FAQ? If not, PLEASE read it. If you haven't read it in awhile, please read it again to see if any updates were made.
Having CCSv5 problems? Check out the CCSv5 Troubleshooting Guide
Click here to track an issue. Enter your bug id in the "Find Record ID" box
Hi,
yes, I am using a DSS script to startup, but the problem was even loading manually with CCS and only with the core2 binary.
Anyhow I found out the root cause, I misconfigured is some way the target configuration moving from windows to linux.
About the other points:
1) libtpitrace.so is missing from CCS 5.0.3 but I saw it is present in 5.1.1.
I simply copied the library and it seems to work even with CCS 5.0.3, but is this a known problem? I could not find it documented
2) about BlackHawk BH560v2 drivers for the kernel 3.2.0-27, does anybody know if they are available?
I saw a note to look for upgrade on CCS 5.1.1 or greater, nothing on CCS 5.0.3
Many thanks!
Kind Regards
Stefano