Hello,
I am attempting to basically re-create one of the example StarterWare projects - the enetEcho example in CCS5. I get to the point of linking, then a bunch of symbols are not found. From Project Explorer, the projects look almost identical, Includes listed, paths etc. I do notice that some basic settings are different - the menu in Project>Properties lists ARM instead of TMS470 (I am targeting the Beaglebone).
Anyhow, I started to just link to all the source files necessary and have removed most of the link issues (unresolved symbols). My question then is - is this the proper way to build a project that is not an example? I am ending up with all the starterware source files listed in my project, and hence this looks nothing like the enetEcho example. I have played around with all the path and project settings I can find to no avail. Is there some common place to have the linker find the starterware object files or something?
thanks!
-ed