Hi,
CCS 5.2.1 installation looks not easy for me. I am trying to install CCS 5.2.1.00018. Last week I downloaded CCS from TI website and saved in a network drive of our company. I unzipped the downloaded file and kept the installation folder in the same folder of the network drive.
Started CCS_Setup application to star the installation on Windows XP 32 bit machine. After completion of Eclipse installation, I stated getting "installation failure" messages. After a while, installation aborted because of too many failures.
Then I referred to couple of E2E discussions on CCS installation failures and tried to unzip the CCS downloaded using different unzip software. Every time same result. I have McAfee installed on the machine and tried to disable that as well. But there is no improvement.
Then I copied the unzipped CCS installation folder to the local machine and started installation, this time it worked. By this time I had already uninstalled the unzip software on that machine.
Then I followed the same steps to install on my laptop (windows 7 64 bit). Here also the installation went smooth without problems.
This week I tried to install CCS on some other machine by following the same steps, and the problem appeared again. I am seeing "Installation failure" messages and no luck so far. Can some one help me for a clean CCS5 installation?
Thanks,
Shivakumar
Hi Shivakumar,
is there something different with the non working setup? Did you double check the unzipping? Do you have access to send us the installjammer registry directory contents from the problem install? (this is found under program files or program files(x86))
Have you verified no directories with accented or special characters was used?Best Regards,
Lisa
Hi Lisa,
There is no difference between the non working machine and one of the working machine. Both of them are with Windows XP OS. I have the unzipped folder on the network drive and the plan is to use that folder for the installation for test of the team. I am using the same unzipped folder to install on the non working machine.
Surprisingly, there is no installjammer registry directory! And while installation I have observed the "installation failure" during the following package installations
com.ti.ccstudio.idemain.feature.group
com.ti.ccstudio.workflow.feature.group
com.ti.ccstudio.c5500.feature.group
com.ti.ccstudio.c6000.feature.group
com.ti.ccstudio.c5400.feature.group
I am installing under C:\ti directory.
Let me try a fresh installation and check for installjammer registry directory.
thanks,
HI Shivakumar,
ok, please keep us informed.
Best Regards,Lisa
My two attempts to install CCS5 failed exactly at the same locations (or packages) that i had mentioned in my previous reply. There is no installjammer registry directory. After these failure messages, the installation completes and upon starting the CCS5 application, Eclipse logo appear and eclipse GUI appear. Still no clue what is going on...
Hi Sivakumar,
could you please double check? These would be hidden folders so you may need to unhide them to see and find them.
THanks,Lisa
I found it. Please find it attached
1004.ccsv5.zip
this still seems like it is possibly unzip related. From what I can tell, it looks like the failing parts of your install are using a temp directory with a space in the name (ie documents and settings).
Please see if you can either verify you unzip before installing and see if you can change the temp location used to something with no spaces.
Please keep us informed.
Best regards,Lisa
I have the unzipped folder of the installer in C:\temp directory. I hope this is the temp directory that you are talking about. I have tried the following with no success
Problem solved!!
great, glad to hear you managed to find the fix. We are working on fixing these unzip incompatibilities in coming releases.
All the best with development.
Best Regards,
That sounds good. Thanks for the help to fix the problem.
-Shivakumar
no problem. That's what we're here for.