This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS5.3 new install

I just installed CCS 5.3.

To test it out, I thought I would use a project that I have been working on in the past. This project is described at "http://processors.wiki.ti.com/index.php/Creating_CCS_Project_using_SimpliciTI". I wanted to have two instances of it side by side for comparison. I created the project following the same instructions, so the two setups are identical. During the build it gave me errors I have never seen before:

These refer to unresolved symbols like " __TI_decompress_none" and similar things. The warnings give a hint for the cause: "D:\ti\ccsv5\tools\compiler\msp430_4.1.1\lib\rts430x_lc_ld_eabi.lib" was not found. The next warning says that it is automatically building this library but when I go to the folder I don't see a file with that name:

So it did not create the library after all, or it created it and then deleted it. I any case, it does not show in file manager.

I looked at my project properties to make sure that the run time support setting is correct, and it seems it is:

What's going on here?

Thanks, Shanyi.



2 Replies

  • Guru 130905 points

    Hi Shanyi,

    what version of CCS were you previously using?  There are two things to check first

    - try changing from elf (EABI) to COFF format.

    - please check your include paths and variables as per this wiki

    http://processors.wiki.ti.com/index.php/Include_paths_and_options

    Please keep us informed.

    Best Regards,
    Lisa

  • Guru 130905 points

    In reply to Lisa TI:

    Hi Shanyi,

    just thought I would check whether there is any update with your enquiry.

    Best Regards,

    Lisa

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.