This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS 5.3.0 update, required items could not be found

When updating from within a fresh 5.3.0 installation I get this:

Cannot complete the install because one or more required items could not be found.   Software being installed: SYS/BIOS (IDE Client) 6.34.2.18 (com.ti.rtsc.SYSBIOS.product.ui.feature.group 6.34.2.18)   Missing requirement: SYS/BIOS (IDE Client) 6.34.2.18 (com.ti.rtsc.SYSBIOS.product.ui.feature.group 6.34.2.18) requires 'com.ti.rtsc.SYSBIOS.product.ui [6.34.2.18]' but it could not be found

 

 

 

7 Replies

  • Guru 130905 points

    Hi Davor,

    did you install BIOS support when you did the 5.3 installation?   Do you need BIOS?  I ask because one immediate work around if you don't use BIOS is to disable those updates in Window->PReferences->INstall/update->Available Software sites. 

    Might you be willing to zip and send the install logs?  THese are in the installjammer registry folder which is  a potentially hidden folder in program files or program files(x86)

    Best Regards,

    Lisa

  • In reply to Lisa TI:

    I did a fresh reinstall and the problem has changed. Now, instead of failing to update, every time I do check for updates it lists:

      DSP/BIOS (IDE Client) 5.42.0.07 com.ti.rtsc.DSPBIOS.product.ui.feature.group

      SYS/BIOS (IDE Client) 6.34.2.18 com.ti.rtsc.SYSBIOS.product.ui.feature.group

      System Analyzer (UIA Target) (IDE Client) 1.1.1.14 com.ti.uia.product.ui.feature.group

     

    Size 0kb. Install, restart, check for updates and they are there again.

     

     

  • In reply to Davor:

    More details.

    Upon starting, CCS found a new product MPS430ware 1.30.0.15 (although it seems to already have been installed). After allowing it to install, I am back to the original problem. The list of available updates is now:

    DSP/BIOS (IDE Client) 5.42.0.07

    Grace (MSP430) (IDE Client) 2.0.1.65

    IPC (Multicore and I/O) (IDE Client) 1.25.0.04

    MSP430ware (IDE Client) 1.30.0.15

    RTSC/XDCtools (IDE Client) 3.24.5.48

    SYS/BIOS (IDE Client) 6.34.2.18

    System Analyzer (UIA Target) (IDE Client) 1.1.1.14

     

    This list now appears every time I do check for updates.

     

  • Guru 130905 points

    In reply to Davor:

    Hi Davor,

    what OS are you running?  Would you be able to send the install logs from the installjammer registry directory?  Would you be able to check for antivirus interference?

    A few tips

    - if you are using LInux, we have seen this type of behaviour if CCS is launched with different permissions as installed.  Ie launched as user but installed as sudo.

    - you can check and verify what and were CCS is looking for these features in Window->Preferences->Code Composer Studio->RTSC->Products

    - if you use Win 7 try to use directories with no spaces or accented characters

    Please keep us informed.  The logs would really help.

    Best Regards,
    Lisa

  • In reply to Lisa TI:

    I had a similar issue a week or so ago. I did updates and it caused all sorts of problems (don't have the detials anymore), so i did a clean reinstall of CCS 5.3.0. Following that, I did updates again. Everything except IPC (Multicore and I/O) (IDE Client)    1.25.0.04 updated fine. I have tried again today, but it still says some required components cannot be found at the update site. Other than that, things seem to be working ok.

    Regards, Leigh

  • Guru 130905 points

    In reply to LEIGH PRINGLE:

    Hi Davor,

    just thought I would double check for any updates with your enquiry.

    Best Regards,

    Lisa

  • In reply to Lisa TI:

    Hi Lisa,

    I've attached the eclipse log file.

    5618.eclipse.log

    Regards,

    ~ Harsha ~

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.