This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

  • Resolved

LM3S8962 Basic Assembly Project

Hi All,

I am trying to get a simple assembly language program setup in Code Composer 5. I have the option to start an empty assembly language project. And I am trying something very simple:

                  .text

start:         ld   r0,#2

                  ld    r1,#3

                  add r2,r1,r0

stop:          b stop

It's as simple as it gets. But I can't get it to compile properly. It keeps complaining about stack and other stuff as well.

I know that I am missing something very simple. The stack for once that needs to be initialized. And maybe some other stuff too.

All I am trying to do is get some very simple assembly code up and running and debug it on my LM3S8962 board.

Any help is greatly appreciated.

Thanks! 

  • Guru 144285 points

    mouka zwina
    But I can't get it to compile properly. It keeps complaining about stack and other stuff as well.

    What are the exact errors you are getting? If you can copy and paste the full error message from the CCS build console that will be helpful.

    When you create the new project are you selecting the "Empty Assembly-only Project" template from the list of templates? This would be the appropriate one to select for a project that is going to contain only assembly source files and no C source file. From there on you should be able to add your source file and build.

    ____________________________________________________________________________

    Please click This Resolved My Issue if the reply answers your question.

    Search the wikis for common questions: Compiler, CCSv6, CCSv7
    Track a known bug with SDOWP. Enter the bug id in the "Find Record ID" box

  • In reply to AartiG:

    That's exactly what I did.

    1. I created a new Empty Assembly Project.

    2. CCS did create an empty project for me.

    3. I added a simple .asm file containing the code I showed before.

    4. I tried assembling, but the assembler, or the compiler, complained about all kinds of things missing or undefined.

  • Guru 144285 points

    In reply to mouka zwina:

    If you can post the complete output of the CCS build view we can try to explain what the errors mean and what could be causing them.

    Was the code snippet you attached the full assembly source file? When you created the new project in CCS, did you pick Stellaris LM3S8962 as the device variant?

    ____________________________________________________________________________

    Please click This Resolved My Issue if the reply answers your question.

    Search the wikis for common questions: Compiler, CCSv6, CCSv7
    Track a known bug with SDOWP. Enter the bug id in the "Find Record ID" box

  • In reply to AartiG:

    Here's all the code I had in my main.asm:

                 .text
    start:
                  mov r0,#1234
                  mov r1,#5678
                  add r2,r1,r0
    stop:     b stop

    here are the errors:

    warning #10204-D: automatic RTS selection: could not resolve index library "libc.a" to a compatible library
    error #10198-D: no input section is linked in

    "../lm3s8962.cmd", line 44: error #10104: undefined symbol "__stack" used in expression
    >> Compilation failure
    warning #10202-D: no suitable entry-point found; setting to 0
    error #10010: errors encountered during linking; "junk.out" not built
    gmake: *** [junk.out] Error 1
    gmake: Target `all' not remade because of errors.

    **** Build Finished ****

  • In reply to mouka zwina:

    The quick-and-dirty answer is to change "start" to "main", and add a ".global main" directive (don't forget to indent it).  You'll get a bunch of startup code that you don't really need, but that's probably the easiest path for now.

  • In reply to Archaeologist:

    I just did. I added ".global main" directive. Without the double quotes obviously. But I am getting the same error messages as I did before.

    I think it is compiling my project as if it were a C project. The reason I am saying this is because it is trying to link the object code with libc.a. 

    I don't even know if CCS is capable of assembling simple projects. It seems that gcc is always trying to compile stuff as a C project.

    I tried several blank projects. But I am always getting the same errors. I tried changing stuff to address the errors I am getting, only to generate a lot more errors.

  • In reply to mouka zwina:

    Please do a "build all" and show us the entire contents of the build console window.

  • In reply to Archaeologist:

    **** Build of configuration Debug for project Test ****

    "C:\\ti\\ccsv5\\utils\\bin\\gmake" -k all
    'Building file: ../main.asm'
    'Invoking: ARM Compiler'
    "C:/ti/ccsv5/tools/compiler/arm_5.0.1/bin/armcl" -mv7M3 --code_state=16 --abi=eabi -me -g --include_path="C:/ti/ccsv5/tools/compiler/arm_5.0.1/include" --diag_warning=225 --display_error_number --diag_wrap=off --preproc_with_compile --preproc_dependency="main.pp" "../main.asm"
    'Finished building: ../main.asm'
    ' '
    'Building target: Test.out'
    'Invoking: ARM Linker'
    "C:/ti/ccsv5/tools/compiler/arm_5.0.1/bin/armcl" -mv7M3 --code_state=16 --abi=eabi -me -g --diag_warning=225 --display_error_number --diag_wrap=off -z --stack_size=0 -m"Test.map" --heap_size=0 -i"C:/ti/ccsv5/tools/compiler/arm_5.0.1/lib" -i"C:/ti/ccsv5/tools/compiler/arm_5.0.1/include" --reread_libs --warn_sections --display_error_number --diag_wrap=off -o "Test.out" "./main.obj" -l"libc.a" "../lm3s8962.cmd"
    <Linking>
    warning #10204-D: automatic RTS selection: could not resolve index library "libc.a" to a compatible library

    >> Compilation failure
    error #10198-D: no input section is linked in
    "../lm3s8962.cmd", line 44: error #10104: undefined symbol "__stack" used in expression
    warning #10202-D: no suitable entry-point found; setting to 0
    error #10010: errors encountered during linking; "Test.out" not built
    gmake: *** [Test.out] Error 1
    gmake: Target `all' not remade because of errors.

    **** Build Finished ****

  • In reply to mouka zwina:

    Just for clarification: I went into the lm3s8962.cmd and I removed any references to the stack since I don't need it to be configured in an assembly project. But then I started getting errors relating to libc.a

    I removed any reference to libc.a from my project settings, and I still couldn't build the project properly.

    I have Googled CCS and I have found some stuff online relating to CCS 4. I have installed CCS 5. I don't know what happened when stuff got moved from version 4 to version 5. But I know for sure that an assembly project selected from the default CCS 5 templates does not work. Too many settings were not done properly.

  • Guru 144285 points

    In reply to mouka zwina:

    Please take a look at this related thread. http://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/176351/637520.aspx#637520

    Although that one is for a MSP430 device the errors noted there are similar. If you add the .retain directive in your asm source file you should be able to get rid of the "no input sections linked in" error. You would also need to set the entry point in the linker options (--entry_point) probably to "start" in your case. And comment out the line that sets __STACK_TOP in the linker command file lm3s8962.cmd. I beleive this should allow you to build without errors.

    Most users begin with C programs, and the out of box templates and examples are set up to work better with C projects rather than assembly only projects. If you plan to run code on a Stellaris LM3S8962 eval kit, the Stellarisware examples are a great starting point.  I would advise taking a look at and starting with the examples there as they are specifically targeted to run on the eval kit.

    ____________________________________________________________________________

    Please click This Resolved My Issue if the reply answers your question.

    Search the wikis for common questions: Compiler, CCSv6, CCSv7
    Track a known bug with SDOWP. Enter the bug id in the "Find Record ID" box

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.