Hi folks,
I am using the MSP-FET430UIF for programming via JTAG into a custom target board based on MSP430F5438A.
The custom board is to be powered via the FET (PIN 2 is connected)
The error I get on programming is "Error connecting to target, unknown device".
I cant say I am 100 percent sure of my PCB, but I have checked in every possible way.
All the connections are as per the Hardware tools guide. Even the voltage from the FET is 3.2V. But still I am not able to program.
I have similar problem when programming the MSP-EXPF5438A experimenter board, when set to FET power.
The error given is "Failed to load program".
But when this experimenter is set to USB power, it can be programmed correctly.
I cant do the same in my custom target board.
Can someone point me in the direction of solving the problem?
The firmware version on FET is 3.02.04.005
Regards
Shashank