Hello,
I had to upgrade to CCS-5.4 for bug fix.
Now I run into another problem where it takes too long to load register while almost instantly with CCS-5.2
Any idea ?
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Ki,
I'm using AM1808 as below.
I just found out it's a lot worse when I'm NOT able to copy and paste register content from Register window to text editor.
I did verify it works great with CCS-5.2, but not CCS-5.4
Thanks,
How are you loading the register? Could you provide detailed steps to describe exactly what you are doing?
1) Open CCS
2) Select CCXML
3) Debug project
4) Wait for GEL file fully loaded
5) Click tab : View - Registers
6) Expand any module, say SYSCFG0ARM
For CCS-5.2
a) All register data appear instantly right after expanding
b) Able to select, copy and paste register data into text editor
For CCS-5.4
a) It takes long time to display register data after expanding a module
b) Able to select register data, but NOT able to copy and paster to text editor
It behaves the same for both OMAP-L138 and AMN1808
Thanks,
Thanks for the steps. Are you using an XDS100v2? That is the only emulator with I see any difference with. XDS510USB and XDS560v2 seem fine.
Duy-Ky Nguyen88210 said:If it does not work with CCS-5.4,
XDS100v2 is fully supported by 5.4. I never said it does not work.
I can reproduce this fairly easily. I will have the engineers take a closer look at this.
Thanks
ki
We're in critical time in preparing a demo to potential customer pretty soon and we have quite some bugs to work on
Recently I got some tool issues slowing down our progress significantly
Please let me know the fix as soon as you can
Thanks so much for your great support, Ki
~Duy-Ky
Duy-Ky,
We have been looking at this and cannot reproduce the second issue you reported about unable to cut and paste. I have no issues with cut and paste from the register view to notepad using CCSv5.4 and XDS100v2 with OMAP L138. Is this still an issue?
Regarding the first issue, I see about a ~3 second lag for expanding the register view with some slow painting in filling in the values. Is this around the same time you observed?
Thanks
ki
Hi Ki,
I tried both on my 32-bit Win_XP Pro and 64-bit Ultimate Win_7 and have exactly the same behavor. They are new PC, only 2 years old
For CCS-5.4
* 32-bit Win_XP Pro : display SYSCFG0ARM lags : 1'47"
* 64-bit Win_7 Ultimate : lags 35"
But, once high-light after full content displayed, right-click on SYSCFG0ARM to select, copy-paste to editor, I got only
========================== Start of Edtitor ============================
SYSCFG0ARM
( BLANK !)
==================== End of Editor ===========================
However, for CCS-5.2, with exactly the same project and CCXML, no lag and copy-paste to editor with full register data
======================== Startof Editor ==========================
SYSCFG0ARM
REVID 0x4E840102 Revision Register [Memory Mapped]
DIEIDR0 0x0901103E Die ID Register 0 [Memory Mapped]
DIEIDR1 0x00639355 Die ID Register 1 [Memory Mapped]
DIEIDR2 0x00000080 Die ID Register 2 [Memory Mapped]
DIEIDR3 0x06400003 Die ID Register 3 [Memory Mapped]
* * * *
================== End of Editor ======================
Thanks,
Sorry, my mistake. I see it now.
I also found some more details. My previous comment that the issues just happen on XDS100v2 is incorrect. It is most noticeable because it is the slowest emulator. I also notice a slight delay with the other emulators (maybe 0.5 seconds). It just isn't as noticeable.
Also the copy & paste appears broken for all emulators
I file a bug for this. Tracking ID: SDSCM00048013
Thanks
ki
Hi,
I have the same problem here. Until a new version of CCS arrives with the fix I use CTRL-X to put a register content into the clipboard or I use the right mouse button to select 'Copy' from the context-menu.
However, I'm anxiously waiting for the fix becaue I always keep forgetting it's not working...
Sincerely
- Peter
Hi Peter,
The issue appears resolved in early versions of CCSv6. Most likely this was already a known Eclipse bug and has been fixed in a recent Eclipse version that CCSv6 picked up.
ki