I get this error whenever I try to build or rebuild or even clean the project. Doing build number of times may some times goes through & finaly once i a while build gets finished. Most od time it shows that build window & keeps me waiting on refreshig project until I cancel it, & on cancel I get this error.
Some times it compiles 1 or 2 files of project & error comes. I have checked for the gmake file, it is there in the said path,
Here is complete error
"../CC1100-CC2500.c", line 107: remark #1535-D: (ULP 8.1) variable "paTableLen" is used as a constant. Recommend declaring variable as either 'static const' or 'const'
gmake: *** Access is denied.
. Stop.
gmake: *** Waiting for unfinished jobs....
gmake: *** Deleting file `CC1100-CC2500.obj'
**** Build of configuration Debug for project RF ****
Command canceled
Error: Program "E:/ti/ccsv5/utils/bin/gmake" is not found in PATH
PATH=[E:\ti\ccsv5\ccs_base\common\bin;E:\ti\ccsv5\ccs_base\common\uscif;E:\ti\ccsv5\ccs_base\DebugServer\license;E:\ti\ccsv5\ccs_base\common\bin;E:\ti\ccsv5\ccs_base\common\uscif;E:\ti\ccsv5\ccs_base\DebugServer\license;E:/ti/ccsv5/eclipse/jre/bin/client;E:/ti/ccsv5/eclipse/jre/bin;E:/ti/ccsv5/eclipse/jre/lib/i386;C:\WINDOWS\system32;C:\WINDOWS;C:\WINDOWS\System32\Wbem;C:\WinAVR-20100110\bin;C:\WinAVR-20100110\utils\bin;C:\Program Files\Microchip\MPLAB C32 Suite\bin;C:\Program Files\Microchip\MPLAB IDE\VDI;C:\PROGRA~1\MICROC~1\THIRDP~1\PICC;c:\mspgcc\bin;C:\PROGRA~1\COMMON~1\AUTODE~1;C:\Program Files\HI-TECH Software\PICC\PRO\9.65\bin;C:\Program Files\Microsoft Visual Studio\Common\Tools\WinNT;C:\Program Files\Microsoft Visual Studio\Common\MSDev98\Bin;C:\Program Files\Microsoft Visual Studio\Common\Tools;C:\Program Files\Microsoft Visual Studio\VC98\bin;;C:\Cygnus\arm-tools\bin;C:\Cygnus\Bin;;e:\Program Files\H-JTAG V0.3.1;C:\Program Files\Texas Instruments\CC Essentials
2.0\eclipse\plugins\com.ti.eem.wrapper_2.0.0;C:\Program Files\Common Files\Ahead\Lib\;E:\ti\ccsv5\eclipse;]
**** Build Finished ****