One of custimer is facing a strange issue, they are trying to run the Test APP with SDP VG1.0.0 ( ES2 , 3430 ) , while they are able to Connect / open both Cortex A8 and C64 both , and they are able to load the code as well .
They are seeing the different behaviour at different run [ test app is DSP based ].
a) Many a times , after loading the program ( DSP ), it automatically starts running [ Window shows that it is running ] [ it doesn't go to main , as the option is selected ] , although It doesn't hit the break point.
b) Many a times , at single step , instead of returning from the function , it goes down and start executing the functions ( which are not at all called )
c) Sometines it works fine [ as no problem ...I tried a sample program which is executing fine ].
It is very inconsistent .
SDP : 3430 ES2.0
CCS : 3.3.77DSP/BIOS : 5.33.02
CGTOOLS : 6.0.7
Board : Blackhawk PCI560 - RevD OMAP3430
I am able to run the same test app with SDP VG5.0.1 without any problem.