Hi Lisa,
I've had a similar problem and I have now downloaded xdias_7_24_00_04.
It's a huge file full of many different file types. What do I install?
Thanks,
Matthew
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Lisa,
I've had a similar problem and I have now downloaded xdias_7_24_00_04.
It's a huge file full of many different file types. What do I install?
Thanks,
Matthew
Hi Dave,
David Elvig said:md/DSP2802x_Headers_nonBIOS.cmd" "../F28027_FLASH_FlashingLeds.CMD"
It looks like two linker command files are being used in your project and they likely have conflicting information. Did you mean to have both cmd files in the project?
Thanks
ki
Thanks. I deleted a .CMD from from the project (one that was higher in the project, and included the word "RAM") which appeared to have the memory ranges with which the Flashing Lights demo was conflicting. Now it builds without error.
Now I try the next step in the F2802x Flashing LEDs Project
Step 3, Debugger Configuration...
I press this and get an 11-item list,
- starting with "Data Snapshot Viewer",
- ending with UART Connection,
- and having 8 "Texas Instruments.... Probe"
- and one "Texas... cJTAG with external converter"
I've tried 4 of them, including one ending in onboard debug probe.
None of them seem to "stick" as my choice (even when pick in Project Properties", and all lead to this error when pressing "Debug the imported project"
Can't Initialize Target CPU:
**Error**: Serial Communication failed at port: COM65, baud rate:9600!
To use serial monitor, please ensure the following prerequisites are satisfied:
1. Make sure the cable is plugged into both the target and the host on the right COM port.
2. Make sure a compatible target side serial monitor is loaded and running on the target device.
Does that make sense?
Thanks
David Elvig said:- I still needed to remove an extra CMD file from my project (that was added at the start from ControlSuite). It included the word ...RAM... and had similar low-memory (zero memory range) addresses that were being mapped.
I imported the project myself and noticed that there are three cmd files listed in the Project Explorer: DSP2802x_Headers_nonBIOS.cmd, F28027_FLASH_FlashingLeds.CMD, and F28027_RAM_FlashingLeds.CMD. The last one is automatically excluded from the build. It is that one that has conflicting information with the first one. Since you it already excluded by default, you should be able to just build right after import and it should be successful (at least it was for me). Is that file not excluded from the build for you when you import it?
As for tutorials, I strongly suggest taking a peek at the CCSv6 beginner workshop for F2802x LaunchPad. It will help you get started with CCS on your LaunchPad:
For training that focuses on the actual hardware more than just CCS, see:
Thanks
ki