Hi
Does CCS 5.5.0 supports C++11. What version of GCC is it based on?
Best Regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
Does CCS 5.5.0 supports C++11. What version of GCC is it based on?
Best Regards
Hi Juliano,
CCS v5.5 does not support C++11.
Refer this link for more info: http://processors.wiki.ti.com/index.php/Overview_of_C%2B%2B_Support_in_TI_Compilers
Regards,
Gautam
Thanks for the answer!
Do you know if Code Composer 6.0.0.00156 supports it? I really need one Toolchain that supports C++11 to work with the Cortex-M3 in the Concerto MCU.
Regards
The TI compiler does not. But CCSv6 also comes with GCC 4.7.4 which looks like it has some support:
http://gcc.gnu.org/gcc-4.7/cxx0x_status.html
Thanks
ki
The problem is that when I create a new project on the CCS6 and I select the GNU V4.7.4 as the compiler (that would support C++11), it says that my device does not currently supports the GNU toolchain, it only supports the TI compiler. I'm using the F28M36x Concerto on TMDXDOCK28M36 Experimenter's Kit. :(
Yes, Juliano GNU toolchain does not support C2000 mcus. An extract says:
Additionally, a department at the Chemnitz University of Technology has developed preliminary support for the TMS320C6x series in the GNU Compiler Collection.[4]
Regards,
Gautam