Hello
I have DM8168 EVM from (Spectrum Digital). I wanted to run a test encoder app on M3 video. I see two JTAG connections on the board. One with 20 pin and another with 14 pin(MSP430). Which one I should use?
For using only M3 Video+HDVICP, what are the steps required? Do I need to boot up the other cores using the SD card, before loading the firmware on M3 video?
Best Regards
JK