I have been using CCSv3.3 on Windows 7 with the XDS510LC USB emulator to program many projects using the TMS320LC2406A for about two years now without too many issues.
So in typical fashion, the production needs boards updated to ship and I find I can't program, getting the following error.
Error connecting to the target:
Error 0x80000A00/-1134
Fatal Error during: OCS, Timeout,
Processor timeout, device would not respond.
Code Composer is Auto Retrying.
Press Cancel button to cancel the current operation.
I/O Port = 510
Board Name: F2406A XDS510USB Emulator
Cpu Name: cpu_0
Abort: Close Code Composer Studio.
Retry: Try to connect to the target again.
Cancel: Remain disconnected from the target
Diagnostic: Run diagnostic utility.
The last boards I programmed successfully was about two weeks ago and the tools/programmers haven't changed in that time (especially since CCSv3.3 isn't being worked on). I am able to talk to the emulator and it is trying to talk to the micro as I see the indicators change on our board that the micro is being reset. Can anyone please provide details on this error code and what may have changed? A few things I have tried already:
- Used three different programmers, including one bought brand new last week.
- Tried programming several of our board designs including the ones I successfully programmed two weeks ago.
- Tried powering the board in test fixtures and in the product.
- Tried other computers that have CCSv3.3 still on them.
- Tried SDFlash utility
I saw one other post that asked this question but it was never answered. I don't think the problem is in the IDE specifically and I would love to move to the newer development tools but they don't support this micro (and the replacement micro is not drop in functionally equivalent.)
Tim