I can't start a grace project on CCS 6.0.0.00190 , I am having the evaluation version. I installed grace from the app center. But now I cant see the option to start a grace project in the new project wizard.
Please help
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I can't start a grace project on CCS 6.0.0.00190 , I am having the evaluation version. I installed grace from the app center. But now I cant see the option to start a grace project in the new project wizard.
Please help
I am using CCS v6.0.1.00040. I have installed Grace from the Apps Center. The Grace tools are installed into CCS. However, when starting a new CCS Project, the "Empty Grace (MSP430) Project" option is not available.
Question: How do I add this entry into the new project Wizard?
Thanks.
From the Getting Started window, Select the App Center. Then select the Grace 3.0 tools, download and install them. The Grace tools are now able to be used as a stand-alone app, that is intalled into CCS v6.0 or later.
Under Project --> Properties --> General --> "RTSC" tab, check the boxes for Grace inclusion.
The Grace project selections are available after installation.