Hello,
Anybody know the CCS how to output or display checksum value in below image? thanks very mcuh.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Anybody know the CCS how to output or display checksum value in below image? thanks very mcuh.
Hi,AartiG
Sorry for I'm unresponsive comfirm your answer, it's correct. But now I have another quessiton is how to calculate option segment checksum of Flash , example: I want to caculate Flash A and B segment only then how I to do? thanks very mcuh.
Xiaowei Bai1 said:But now I have another quessiton is how to calculate option segment checksum of Flash , example: I want to caculate Flash A and B segment only then how I to do?
Sorry but there is no option in the tool to calculate the checksum for each flash sector, it is only calculated on the entire Flash.
Hi AartG,
Thanks for your prompt reply! Now I realized that this is probably not related to CCS version. I'm using F28377D and the button "Calculate Checksum" is nowhere to e found, as shown in the attached screenshot. But if I connect it to an older device F28069, it would show up fine.
The question now is, how to get it to work for F28377D?
Harry said:I'm using F28377D and the button "Calculate Checksum" is nowhere to e found,
I don't see it for the F28377D device either. It must be something device specific that dictates whether this feature exists in the on-chip flash tool or not. I would suggest asking in the C2000 forum as the experts there should able to comment further.