Hi experts,
I am using CCS 5.5 (C6000 codegen tools v7.6.0) for building our project, which consist of a main executable project and 15 dependent static libraries. I was wondering if it is perhaps possible to somehow shorten the rebuilding time when doing development. Currently it can take up to 3-4 minutes to perform a rebuild when only making changes to a single source file. This is due to every dependent project first being checked for changes. Although this checking is necessary and to be expected, I do feel it takes much longer than it should, especially since I am using an i7 processor and have lots of RAM on my PC.
Since the static libraries are inter-dependent, I cannot simply remove them as dependent projects from the main project.
Is there anything else I can do to improve the rebuilding time?