Hi,
I am using Cose Composer 5.5.0.00077
For the TMS 28346 compiler version : TI v6.2.7
Sometimes, when pausing the debugger, the following error appears :
Can't find a source file at "/tmp/TI_MKLIBNoWO2Z/SRC/fs_div28.inc"
Locate the file or edit the source lookup path to include its location.
When resuming everything seems to be correct.
I've find that this file is on c:\ti\ccsv5\tools\compiler\c2000_6.2.7\lib\src\
I have seen an old post:
"0 FS$$DIV() at fs_div28.inc: 212 0x3f6d6a" from 17/5/2012 (CCSv4)
that indicates that this error may be “dismissed “.
Is that still true for CCS-v5?
I am using the following libraries:
"rts2800_fpu32.lib"
And I use floating point Division.
Thanks a lot.