Hello,
I have big troubles with the latest CCS (Version: 6.0.0.00190) : when I create a new workspace I can compile and debug my projects , but after closing and reopening my workspace it is no more possible to compile and debug, and in the console I have :
Cannot run program "make" : Launching failed
Error: Program "make" not found in PATH
I tried several times to reinstall (uninstall, delete directory...), no improvment. I tried on 2 different computers (Windows Seven 32bits and 64 bits) with the same result again.
The only mean to work (because I need to produce ...) is to delete the .metatdata directory, then opening my workspace (thus create a new one) and then import all my projects in this workspace. I have to repeat this operation each time I open a workspace, It is really tricky.
So, please, I need some suggestions to workaround this problem.
I also notice that to create .txt file I obtain a .hex file, but it seems to be already a known issue.
Thanks
Peter