Hello,
I have some questions about debug probe for three c6671s.
Q1> If three DSPs are independently connected to debug probe like 'device-independent trace configuration', can CCS access three DSPs at once?
Q2> Can I use either XDS100 or XDS200 for debugging c6671? If I can, what is the restriction comparing to XDS560v2?
Q3> Can I configure single or parallel trace by XDS200?
Q4> c6671 has 19 emulation ports(EMU00~EMU18). When I configure trace with XDS560v2, should I connect all emulation port pins? What is minimum pin number for signle/parallel trace?
Q5> When I configure parallel trace with XDS560v2, what is the advantage comparing to single trace?
Q6> When I connect three DSPs over SRIO or PCIe for sharing each DSP's memory, which trace configuration can access all memories of three DSPs?