Hi everyone,
I wish to do image algorithm emulation via JTAG in c674x dsp core, which is one core of dm8148. These days i do a easy experiment by running a "Hello World" program. However I meet a problem. After connecting to dsp core and loading program, dsp is running to a wrong state.The gel i use:44848.DM8148_EVM.gel .
A piece of my program map:
//----------------------------------------------------------------------------------------------------
OUTPUT FILE NAME: <dm8148Emulator.out>
ENTRY POINT SYMBOL: "_c_int00" address: 800078e0
MEMORY CONFIGURATION
name origin length used unused attr fill
---------------------- -------- --------- -------- -------- ---- --------
IRAM 10800000 00040000 00000000 00040000 RW X
OCMC 40300000 00020000 00000000 00020000 RW X
DDR3_RAM 80000000 10000000 0000e62e 0fff19d2 RWIX
//-------------------------------------------------------------------------------------------------
After connecting to dsp, before loading program:
After loading program: