Hi,
I am using CCS5.5. I doing device debugging of project-less target C67xx. To Target Configuration file, I am providing the path of my own GEL file as initialization script. The GEL file Contains the Startup function. In the Startup function I am doing Memory Map Setup.
When I am Launching the Debug session by using the Target Configuration file, the console is populating the error message "Error while executing StartUp(): Could not write 0x01800000: Target is not connected at *((int *) 0x01800000)". I am connecting the Target after Launching the Debug Session. Same GEL file worked fine on the CCS3.1 without any error massege. How to avoid this error message in CCS5.5?
Thanks,
Manish