hi,
we at our Company intend to buy CCS License and have few questions about it.
Our scenario is as follows.
- CCS5 / CCS6
- C2000 DSP
- Jtag-Jet Debugger
- Xds100 Debugger
1. I need to debug two different hardwares at the same time with Jtag-Jet, for that I am going to use either two machines or a single (which ever work fine).
2. I also do other projects where I don't need Jtag-jet just an XDS100 will do the job.
I thought of buying a Single FLoating or Node locked license and have few doubts to clear.
I intend to use CCS5(Jtag-jet don't work with CCS5.5 or higher) and CCS6.
Is it possible to run CCS5.x and CCS6 from same floating License and License server?
Is it possible to run CCS5.x and CCS6 from same node locked License?
Can I open multiple Instances of CCS (e.g CCS5.4 and CCS6) on same machine, at the same time, using single floating/node-locked license? In case not can I install CCS5.x with paid license and CCS6 with free license or vice versa?
On this page
http://processors.wiki.ti.com/index.php/Licensing_-_CCSv6
it says that a SIngle user node locked license can be used on two machines at same time, can I do the same with floating license? (i-e same user logged-on two machines at same time running CCS utilizing just one license?)
Thanks and regards.