I have been happily running CCS v5.3 on a windows 7 machine for a few years now. I've been building boot code for a TMS570 and using a Spectrum Digital XDS510 USB to program the device over JTAG. Today I downloaded CCS v5.5 (I wanted support for parallel compilation). I was happy to see that, once it had installed, all my workspaces were available and all my debug configurations were available without me having to import or create them. BUT.... when I tried to download a boot image to the TMS570 it downloaded OK but would not run! I finally tracked the issue down to an unchecked tick box in the debug configuration... it was the one for Auto ECC Generation.
I reproduced this on a colleagues machine. On his CCS v5.3 I checking that Auto ECC Generation tick box was selected, I upgrading to CCS v5.5 and then saw that the Auto ECC Generation tick box was now not selected.
Installation bug? Or maybe v5.5 does not interpret v5.3 generated debug configurations?