I have a node locked CCSv6 license, which was working on the primary and remote hosts. The primary host was replaced and so the license file was updated, with the primary nodeid and hostname changed.
The updated license file worked on the new primary host, but on the remote host (which hasn't changed) got a flexlm error that the hostid was incorrect:
Where the remote hostid is the second one and matches the MAC address of the wifi interface in the laptop. I think the error is that CCS 6.0.1.00039 under Linux (CentOS 6.5 64-bit) is failing to detect the hostid. If I go to the License Setup Wizard on the remote host the host ID reported is incorrect:
[The License Setup Wizard on the primary host which does accept the license shows the hostid correctly]